5/4/2020 8:23 PM | |
Posts: 24 Rating: (0) |
Hello All, I have CPU 1200, and I want to change the IP address of the PLC and HMI from 192.168.0.1 , .02 to 192.168.1.197 ,.198. I did change the IP addresses of the PLC and HMI in such a way that they are connected together.BUT, since it needs to stop PLC, after downloading the new hardware change, I COULD NOT change the PLC mode from stop to run mode. I tried, power off and on, downloading full software, memory reset, but by either way, I could not change the mode to run mode, and I had to bring back the IP address to old one and download again to be able to change the mode to run mode. Does anyone have a similar experience? Thanks in advance for any advice. Esi ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/05/2020 06:43:51New subject after splitting |
|
Follow us on