9/5/2016 5:28 PM | |
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating: (15) |
When i change it to PLC_1 then i click on evter it changes it to PLC_2 |
9/5/2016 5:31 PM | |
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating: (15) |
PLC |
9/5/2016 5:33 PM | |
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating: (15) |
drive |
9/5/2016 5:39 PM | |
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating: (15) |
. |
9/5/2016 5:41 PM | |
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating: (15) |
The others are the same but instead of port 1 its port 2 |
9/5/2016 5:55 PM | |
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating: (15) |
Both the ports are giving me an error, im going to try and load the ports that arnt loaded |
Follow us on