11/13/2020 7:40 AM | |
Joined: 6/19/2019 Last visit: 4/5/2024 Posts: 690 Rating: (72) |
Hello, If you whant 4.4 firmware you can download here. If you don't have TIA V16 use with your TIA latest firmware what exist. |
Last edited by: Jen_Moderator at: 11/13/2020 12:15:51Optimized link. |
|
11/13/2020 7:45 AM | |
Joined: 5/9/2020 Last visit: 8/29/2022 Posts: 3 Rating: (0) |
My friend, have last updates TiaPortal 16 update 3 and he cant search firmware 4.4 for this IM. |
11/13/2020 7:50 AM | |
Joined: 6/19/2019 Last visit: 4/5/2024 Posts: 690 Rating: (72) |
Try to download from link there I shared |
11/13/2020 8:27 AM | |
Joined: 5/9/2020 Last visit: 8/29/2022 Posts: 3 Rating: (0) |
Oh thanks, i think what if instal GSD file he update module, but he all new gsd files in other devices. |
11/14/2020 9:41 PM | |
Joined: 9/21/2012 Last visit: 4/24/2024 Posts: 3916 Rating: (444) |
Even if you can only select v4.2 from the HW catalogue, you can still use the new 4.4 module without any problems. |
11/14/2020 11:06 PM | |
Joined: 3/30/2020 Last visit: 4/24/2024 Posts: 4440 Rating: (926) |
Hello. @Hati is correct with his answer. You can use the device as if it is firmware version V4.2. You do not need the firmware, to update your TIA Portal. The hardware descriptions of TIA Portal V16 needs to be updated. That can be done by loading the newest Hardware Service Pack which can be found.. Specifically it is HSP 0318 that you need. Do notice that the download has export restriction so you need to be registered for that separately. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on