1/22/2019 6:37 PM | |
Joined: 12/10/2018 Last visit: 10/22/2021 Posts: 2 Rating: (0) |
Hello, the offline-trends of my 3rd-party-devices (Saia-Burgess-Controls) aren't collected automatically, manually collecting the data works. Could this be because of a wrong notification class/ alarm-priority? At the moment the device should send notifications to NC90/ priority 193. I imported the ede-file without configuring new templates, simply using the automatically assigned "BA_Device_BACnet_HQ_1". The attachement contains the configuration of a TR + NC-objekt. Thank You. Attachmentbacnet-trend.txt (344 Downloads) |
Follow us on