6/2/2020 11:19 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, Yes it is possible. But you have to do a little trick. Should I tell you? …... OK, here it comes: Insert a simple And or Or block and connect it to the variable where SFC Access is configured. Drag and drop the interconnection to the new location. A popup will be shown where you must confirm if you want to move the SFC connection as well. Click Yes/Apply and the SFC access is changed to the new location. Remove the interconnection to the And/Or block again and you're done. |
If I could help you, you can use the RATE button. Thank you. |
|
6/2/2020 1:46 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, I misread your question, I thought you needed to move the SFC access. But yes, copying is not possible. You need to do this manually. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on