4/18/2020 5:43 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, Check my thread at PCS7 Complete Overview and see the links under "APL forum links" |
If I could help you, you can use the RATE button. Thank you. |
|
4/18/2020 6:14 PM | |
Posts: 5 Rating: (0) |
Hi, I already read your post (https://support.industry.siemens.com/tf/us/en/posts/custom-block-icon/151745/?page=0&pageSize=10#post612021 ) but, i wonder that Can I use this feature for own analog/motor etc. block and own wincc block icon? or This feature is just for PCS7. |
4/18/2020 7:42 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, Yes ofcourse you can. I recommend reading the APL styleguide in order to create blocks that fit APL standard. Like using attributes for block, using structure inputs/outputs etc. Very important. When the block is ready, you can create block icon and faceplates. I highly suggest using a existing block icon like a VlvL with it's faceplates because making your own faceplates is difficult. Rather you adjust the faceplates yourself. All can be found under the links I described. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on