12/7/2010 6:16 AM | |
Joined: 4/14/2010 Last visit: 11/17/2020 Posts: 487 Rating:
|
GOOD MORNING Q.1 How can i integrate drive monitor file in simatic manager there are problem with MasterDrive is not open in Simatic Manager Kindly Find Attached Snaps???? Q.2 How Can i recover the MMC data..???? there are hardware error on the simatic MMC. help message 33:8580 can i repair it with any recovery software..???? Thanks Regarded AttachmentDRIVE MONITOR.zip (62 Downloads) |
MS |
|
12/7/2010 7:32 AM | |
Joined: 8/25/2006 Last visit: 1/15/2021 Posts: 2005 Rating:
|
May be you have not installed DriveES package, which allows integration of drives into Simatic Manager. |
12/10/2010 2:29 PM | |
Joined: 4/14/2010 Last visit: 11/17/2020 Posts: 487 Rating:
|
Good Evening Sir Can I copy Past CFC System Block FM 458-1 Program from One to another MMC with USB-Prommer same as procedure (see in attached snaps)....????? After Copy past CFC program It will enough Download for FM 458-1 Module..???? Can I copy Past CFC Program for MMC with the help of SIEMENS Field PG Internal USB-Prommer...???? OR Is the only way to Download Program In ON-LINE & OFF-LINE Mod in FM 458-1 Not More option Like as Copy Past for MMC....???? Because I have Same Application one another Machine I want Copy the CFC program from Its FM458-1 MMC and Past to another FM 458-1 MMC.. Is This Possible.....????? Thanks Regarded AttachmentMMC.zip (74 Downloads) |
MS |
|
12/10/2010 3:41 PM | |
Joined: 4/14/2010 Last visit: 11/17/2020 Posts: 487 Rating:
|
Sir I know i send you CPU 414 Block Memory Snaps Its Just for Example.... I mean Can i copy past CFC program from Running FM458-1 Module MMC & Past it Stop FM458-1 Module MMC Which is Continue Demanding for Program...??? I have try copy CFC Chart from another Machine Program But after Compile the following Message Appear in Logs Window... E: File C:\Program Files\Siemens\Step7\S7cfc\sdblocks\fbamax.a not found. I have search for above file in project folder but not Exist attach snap... Can you Send me a Example project Which has the :Global\sdblocks\fbamax.a File Just for Understanding...???? I have download CFC Example Project from Net But any one have not fbamax.a file.... Thanks Regarded.. AttachmentGlobal.zip (62 Downloads) |
MS |
|
12/13/2010 5:32 AM | |
Joined: 4/14/2010 Last visit: 11/17/2020 Posts: 487 Rating:
|
GOOD MORNING Can you help me how can i replace blocks with CFC project library Find Attached...??? Can you Suggest which blocks i can use from CFC Library for These Blocks (See in Snaps)...???? Can you Send me an Example Project CFC Which have fbamax.a Library File..??? Thanks Regarded AttachmentBlock.zip (53 Downloads) |
MS |
|
Follow us on