11/4/2021 4:05 PM | |
Joined: 12/18/2014 Last visit: 4/18/2024 Posts: 32813 Rating: (4060)
|
How many pulses comes in which time when speed is correct? |
11/4/2021 4:12 PM | |
Joined: 12/18/2014 Last visit: 4/18/2024 Posts: 32813 Rating: (4060)
|
If you mean ... |
11/4/2021 4:24 PM | |
Joined: 11/11/2017 Last visit: 4/16/2024 Posts: 185 Rating: (4) |
yes IF the chain is moving :P |
11/4/2021 4:56 PM | |
Joined: 11/11/2017 Last visit: 4/16/2024 Posts: 185 Rating: (4) |
fantastic and thanks for the heads up. this is something i can work with and suits the application just fine. |
11/4/2021 5:10 PM | |
Joined: 12/18/2014 Last visit: 4/18/2024 Posts: 32813 Rating: (4060)
|
Here's the priciple ... |
This contribution was helpful to1 thankful Users |
Follow us on