6/2/2011 9:27 AM | |
Posts: 34 Rating: (0) |
Hi everyone, I want to change the picture of a standard Block icon in @PCS7Typicals.pdl.. How can it be done? Please help me. Thanks & Regards. Chetna |
6/2/2011 9:54 AM | |
Posts: 691 Rating: (37) |
You can edit the Block Icons. Open @PCS7Typicals.pdl , select the desired Bolock Icon and right click. Choose Coustomized Objects-> Edit, in that you will see an object Status Display showing some pic. You can modify that with the help of its properties. Once you finished editing, select all the Block Icons object , then right click -> Customized Objects -> Finish Editing. Once you do OS Project Editor all the Block Icons resets to by default Configuration How can you create your own block icons that will be incorporated |
6/2/2011 1:59 PM | |
Posts: 691 Rating: (37) |
Dear Chetna The pic you have given is already in Edit mode. The reason that is Dark Black is that it has been used by the Block Icon Property. Please refer to the above posted link for Creating Block Icons. First you close this Pdl without saving anything and then re-open it and then go for edit |
6/2/2011 2:14 PM | |
Posts: 34 Rating: (0) |
Hi, I have done exactly the same way as the procedure is but 'configuration dailog' is not coming active. take a look at the attchment. Thanks. Chetna |
6/2/2011 2:26 PM | |
Posts: 34 Rating: (0) |
Hi Shar. Yes the pic is taken from HMI Symbol Library. Please tell me how is it done. How can we use a picture from Std Library of Siemens? Thanks. Chetna |
6/2/2011 2:41 PM | |
Posts: 691 Rating: (37) |
Go to View-> Library-> Symbol Library or simply search for Symbol Library button on the Graphics Designer Toolbar. Once Symbol Library Window appears browse your symbol and drag and drop into your PDL. Then double click that symbol for editting the properties You can refer this thread also |
6/3/2011 7:47 AM | |
Posts: 34 Rating: (0) |
Hi Shar, I have used a pic from Symbol Library but I am not able apply any action on 'OnClick'Property.. Please tell me how can this be done. Thanks. Chetna |
6/3/2011 8:14 AM | |
Posts: 691 Rating: (37) |
can you please make the properties wider . I can't see it properly |
6/3/2011 9:37 AM | |
Posts: 34 Rating: (0) |
Hi, Please check out the following attachments. Thanks Chetna. Attachmentproperties.zip (163 Downloads) |
Follow us on