6/12/2019 10:59 AM | |
Joined: 4/28/2015 Last visit: 4/22/2024 Posts: 1 Rating: (0) |
Hello, I change value of timer from 1 s to 100 ms (see picture Synchronization 1). When I load modified block to PLC, window of synchronization appear (see picture Synchronization 2). When I click to Offline/Online comparison, I see that safety block DB30001 is different between online and offline version of project (see picture Synchronization 3). But I modified just time of timer. When I click on Continue without synchronization, modified block is downloaded to PLC. But safety program in offline version is inconsistent (see picture Synchronization 4). Few days ago, I changed value of this timer from 2.5 s to 1 s and everything happend good. I tried to modify this timer on 3 different PLCs, but problem is same. Could you help me to solve this problem? Thank you in advance. AttachmentSynchronization.zip (32 Downloads) |
Last edited by: tupek at: 06/12/2019 11:00:20 |
|
6/12/2019 1:56 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi tupek, There is defined procedure for downloading in F system. I guess u should try for Compile changes- Download changes. It should work. U can refer documentation for basic functions. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on