9/5/2005 3:02 PM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating: (32)
|
You wrote: >> It's possible that WinCC detect automatically the server >> when i passed a WinCC project from a computer to >> another? I have the problem that everytime i passed a >> WinCC project to another computer i need to change >> manually the name of the server. This is just possible with WinCC ODK Functions. I have attached you a contact for ODK. ==>>http://support.automation.siemens.com/WW/view/en/9652128 Best Regards Technical Support |
Last edited by: O_Moderator at: 12/14/2010 2:07 PMlink edited |
|
9/5/2005 3:03 PM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating: (32)
|
The WinCC Competence Center Mannheim has developed a tool which allows to rename the computer name from a WinCC project off line. That means, the WinCC project must not be open. The tool is a small exe file which has as parameter the name from the WinCC project. If your are interest, please contact us: WinCC.Competence@siemens.com Michael Alter Siemens AG WinCC Competence Center Mannheim WinCC ODK Hotline Dynamostr. 4 68165 Mannheim Germany Fon: +49 621 456 2265 Fax: +49 621 456 3334 Internet: http://www.siemens.com/process-management |
10/7/2011 9:54 AM | |
Joined: 10/5/2009 Last visit: 1/20/2022 Posts: 2 Rating: (0) |
Dear Michael Alter, I would like to have that tool. Is it free of charge? Giorgos Rigopoulos |
10/7/2011 10:19 AM | |
Joined: 10/3/2010 Last visit: 4/25/2024 Posts: 1552 Rating: (188) |
I don't think they have free tools and it's possible that the wanted tool doesn't exist (work?) anymore for WinCC as it's not in the list, check here: http://www.industry.siemens.de/industrysolutions/de/en/wincc/support/wincc-tools/Pages/Default.aspx |
B r g d s , |
|
Follow us on