6/14/2016 8:56 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi Jackcaress, thats what I expect when I reset the CPU... Have a look in the S7-1200 system manual, chapter 15.5:
hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
6/14/2016 9:20 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
factory-settings means also that the time is resetted to 2004. How could the CPU know the actual time with its factory settings? What you need is a kind of NTP-synchronizing, that synchronizes with an NTP-server. If it is only neccessary to synchronize with panel, this FAQ seems to be perfect for you: Clock synchronization between a HMI operator panel and a SIMATIC PLC hope this helps,, regards, |
FCK WAR! |
|
This contribution was helpful to3 thankful Users |