Industry Online Support
Technical Forum
6/3/2009 8:10 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, I don't believe that you can change the IP address of the CPU via the program. But you can change the IP address of a communication processor CP with the FB55. See in this manual: http://support.automation.siemens.com/WW/view/en/30374198 In chapter 8, they explain how programmed connections work. You can set connections but also some system data for the CP (one item being the IP address). May be you shoud consider to add a CP to your configuartion. |
Best regards |
|