10/31/2011 9:24 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
Hi aterris, AttachmentExample.zip (690 Downloads) |
11/1/2011 7:19 AM | |
Posts: 8 Rating: (0) |
Hi Bigfoot, Ok please find attached some pictures of my configuration and explanation of my problem. 1) The PC Hardware Configuration pic shows the configuration in the hardware configurator in Step 7. 2)IE General IP Address shows the IP address of the IE general in Step hardware configurator (This is where i am able to change the ip address to something new download to the microbox and step 7 configuartion chnages online) 3) Microbox Station Configurator shows the station configuration in the microbox this is where my problem is the IE General IP address never changes here and is always greyed out not allowing me to change it on the microbox also in the network configuration for windows i am unable to change it their it says i need to install and enable a network card which already is. Hope this is more clear for you now. Regards Alan AttachmentIp Address.zip (548 Downloads) |
11/2/2011 11:26 AM | |
Posts: 8 Rating: (0) |
Bigfoot, Ok this is my problem in teh windows network configuration it will not let me change the ip address.See attached more pics. Attachmentpics.zip (580 Downloads) |
11/2/2011 1:04 PM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
Hi aterris, okay now i understand your problem. :) sorry i was on the wrong way Well some questions: Have you tried to Shutdown the Controller and try then to change the IP address? Have it ever worked to change the IP before? Have you tried to Reinstall the Driver for the network card? (Deinstall and then Install) http://support.microsoft.com/kb/308939/en-us Maybe this would help you. I hope so! greetings bigfoot |
11/3/2011 12:28 PM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
Hi, have you tried these two options on the pictures in the .zip-file before? 1. Repair the Network Connection 2. Roll Back Driver Some other user (standard Windows XP user with a normally Computer) have the same problem and on the Windows Website in the forum it says that they have to uninstall and install the driver. If this doesn't help than just take the Recovery CD from your IPC427C and run it. After the Recovery it have to work. Another last crazy idea is: Delete the CP 1616 from WinLC Place the IE General in the WinLC (on IF1 - IF4 dosen't matter) Reboot Delete IE General from WinLC Reboot And then try if you can change the IP Address Must be the same as to Reinstall the Driver. My problem hereis, that i can't reproduce your case. But if you have another idea or the solution for this problem, please let us know :) regards bigfoot AttachmentDriver Options.zip (434 Downloads) |
Last edited by: bigfoot at: 11/3/2011 12:29 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on