8/7/2009 11:27 AM | |
Posts: 48 Rating: (0) |
Hello , We are using S7 -414H CPU with SM modules on ET 200 m racks in I/O Redundancy. While configuring Channel Redundancy CPU goes to stop.I am attaching the Diagnostic buffer along with this as I can't understand the problem. The same system works perfetly on Modular Redundancy. Now I tried the Library IO_CGP_V50 and this problem occured. I checked for the IO cards for their Channel Redundancy Support and they are supportng it. So may be the program is missing something. I wrote program like this OB 1 à FB450 RED_IN ( DB16 ) à My FCs and My FBs à FB451 RED_OUT ( DB17) OB 72 (RED_FLT) à FC450 RED_INIT à FC451 RED_DEPA à FB452 RED_DIAG ( DB18 ) OB 82 (I/O_FLT1) à FC451 RED_DEPA à FB452 RED_DIAG ( DB19 ) OB 83 (I/O_FLT2) à FC451 RED_DEPA à FB452 RED_DIAG ( DB20 ) OB 86 (RACK_FLT) à FC451 RED_DEPA OB 87 (COMM_FLT) à FC451 RED_DEPA OB 100 à FC450 RED_INIT OB 102 à FC450 RED_INIT OB 122 (MOD_ERR) à FC451 RED_DEPA I need to know what I am doing wrong Thanks in advance Nithin
AttachmentDiagnose - Notepad.pdf (187 Downloads) |
Last edited by: Nithin at: 8/7/2009 12:25 PM |
|
10/17/2009 6:49 AM | |
Posts: 48 Rating: (0) |
Sir, It was solved. Again a problem with one of the priority class having less memory. I was in a hurry and so posted this question. Sorry. Anyway thanks. Nithin |
Follow us on