8/7/2012 9:43 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi Well you will have to decide the IO quantity See there are 32 Channel cards and 16 Channel cards for Di or Do. This depends on the project type. Normally you can choose 32 channel cards as you can accomidate 32 di or do signal in one card which can save some cost and space to customer. On the other hand if you choose the 16 channel card then the number of cards will increase depending on the IO's. Eg: For a WTP project you have following IO's DI 432 DO 545 With 32 channel DI cards No of cards = 432 /32 = 13.5 so roughly you can take 14 cards. the same goes for DO. Note that the number of front connectors increase and the number of racks increase If you use profibus protocol then you can have 12 cards in a rack if you use IM 361/IM365 you can have 8 cards in a rack. See the attached excel sheet for calcualting the IO quantity. Have fun... AttachmentMMS_IOLIST_OFFER_TEMPLATE.zip (74 Downloads) |
Jazz |
|
8/7/2012 9:57 AM | |
Posts: 3 Rating: (0) |
Dear Tagolover, thanks so much for your quickly reply. I understood more but could you tell me more clearly,when i choose DO Souring, DO Sinking, DO relay, etc...because i don't understand the application of IO card suitable for which signals Best regards Linh |
8/7/2012 12:46 PM | |
Joined: 9/27/2006 Last visit: 5/7/2024 Posts: 12257 Rating: (2666)
|
Hello babybk; The following FAQ discussses sourcing/sinking IO, the electrical circuitsand the logic signals they use. It will also describe the S7-300 digital IO modules in terms of sourcing or sinking applications. What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC? A more basictheoretical description can be found in Wilipedia: http://en.wikipedia.org/wiki/Sinking_and_sourcing
If the sinking capability of a circuit is exceeded (for example when too many inputs of other gates are connected to it), then the voltage at that point may be too high, higher than that corresponding to a Low state. The circuits then may malfunction.
If the sourcing capability of a circuit is exceeded (for example when too many inputs of other gates are connected to it), then the voltage at that point may be too low, lower than that corresponding to a High state. The digital circuits then may malfunction. |
Last edited by: dchartier at: 8/7/2012 12:48 PM |
|
8/13/2012 5:31 AM | |
Posts: 3 Rating: (0) |
Thanks Dchartier for your Reply, it help me so much |
Follow us on