6/19/2015 10:26 AM | |
Joined: 9/8/2005 Last visit: 4/16/2024 Posts: 8 Rating: (0) |
From the STEP7 error code table: 33:53790 The module to be assigned parameters is currently busy assigning parameters to subordinate devices. It was been by the modules: 416-2DP + CP443-5 Extended
Remedy: reset the CP via Online HW Config and Download HW Config. Repeat the module download when all stations and field devices on the bus are started up and in operation. To ensure that the module to be downloaded temporarily cannot assign parameters to subordinate devices, remove the interconnecting bus cable from the DP interface for the duration of the downloading process. https://support.industry.siemens.com/cs/de/en/view/770453
|
11/7/2015 9:25 AM | |
Posts: 36 Rating: (1) |
Thank you Sevensson , I made a downloading in Stop mode, I think the problem has become after upgrading the System.
|
Follow us on