4/29/2016 2:20 PM | |
Joined: 12/16/2012 Last visit: 9/13/2024 Posts: 653 Rating: (130) |
Hi! I had to add EPLAN to the list. |
4/29/2016 3:02 PM | |
Posts: 1529 Rating: (202) |
Thanks, I was drawing a blank on EPLAN. |
4/29/2016 3:08 PM | |
Joined: 10/2/2013 Last visit: 9/13/2024 Posts: 339 Rating: (52) |
ALL Expert have suggest about Auto CAD and Eplan i am also agree with them, but is there all conditions are satisfy ? asZeid Sinokrot wish like simulation mode? "Is there any programs that are used in drawing control circuits with: PLC, VFD, MOTORS, ENCODERS, SENSORS, push buttons ....and can put them in 3D and simulation mode?" |
Technology is best when it brings people together,so we are here now :) |
|
4/29/2016 4:12 PM | |
Posts: 5225 Rating: (1192) |
Hi friend Jeff, Are you an old dog not learning new tricks?.. Siemens Automation and Drives actually owns a CAD company (actually it is much more than just "CAD"). This company gives away for free the 2D capable software. The catch is that you need to register (not really a hassle for most). The 3D capable software is not for free. Check... I prefer using this software over good 'ol Autocad.. especially because there is a legal free edition but also because of how it works Useful? Late note: Some other packages are available under GNU (free + open) licensing, but it has been a while for me seeing if there is anything worth mentioning. |
Last edited by: William_B at: 4/29/2016 4:14:26 PMadd late note |
|
This contribution was helpful to3 thankful Users |
4/30/2016 2:34 AM | |
Posts: 1529 Rating: (202) |
Old dog - yes Not learning new tricks - No, just wary enough to look at the new trick and ask "You want me to do that? Why?" THanks for the link, I'll check it out. |
This contribution was helpful to1 thankful Users |
Follow us on