8/22/2014 6:32 AM | |
Posts: 5 Rating: (0) |
I am trying to use a clock bit to enable a GETblock at the REQ parameter. I have enabled the use of the clock memory byte and am using that tag. When I monitor the value at the tag it just reads false. I am new to S7 and I wonder if I have a basic setting wrong somewhere. Anybody got an idea what I could check? I have attached my program. Thanks! AttachmentProject30.zip (60 Downloads) |
8/22/2014 8:09 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
It's a TIA v13 project, perhaps you can make some printscreens as well for those who have not installed V 13 (yet). Check the notes Georgio wrote. Faq: How can you avoid overwriting the flags that are allocated for system and clock memory bits in the user program? Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to2 thankful Users |
8/22/2014 8:23 AM | |
Posts: 5 Rating: (0) |
Thank you. That was what I was doing, I was overwriting them another place in my program. Thanks for the help! |
This contribution was helpful to2 thankful Users |
8/22/2014 9:16 AM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating: (14) |
It's a TIA v13 project, perhaps you can make some printscreens as well for those who have not installed V 13 (yet). Check the notes Georgio wrote. Faq: How can you avoid overwriting the flags that are allocated for system and clock memory bits in the user program? Regards, Marcjan I have TIA v13 installed, but I am unable to open the project... but anyway problem solved Regards.
|
Georgio |
|
Follow us on