1/24/2014 7:08 PM | |
Posts: 8946 Rating: (999) |
No! I Timer in OB35 is not a good solution. One posibillity: Change OB35 scantime to 10 ms an use a flag AN "M 0.0" = "M 0.0" |
1/27/2014 5:57 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating: (6) |
I have deleted the OB100 since I only use it in one rung. Attached I have inserted the network that I will use. It is a simple compare instruction to 1. I think it will be simpler to follow the program this way.
AttachmentDocumento4.pdf (245 Downloads) |
Thanks, |
|
Follow us on