Industry Online Support
Technical Forum
2/21/2014 4:39 PM | |
Posts: 2 Rating: (0) |
Hello my friends, I am an intern and I do not have much experience in Industrial Networks. So, I am trying to conect a Toledo IND560 to a S7-1200 CPU through a CM1243-5 as a Profibus DP Master. However, I am not having sucess. I could create the Profibus Network using the GSD file of the IND560. I throught it would work but when I downloaded it to the CPU everything stoped. The status says that the Slave_1 is "not reachable". I checked the cable and it appears to be working properly. AttachmentErros Images.pdf (169 Downloads) |
2/21/2014 4:45 PM | |
Posts: 8946 Rating: (999) |
Adress setting of Toledo is OK? (DIP-Switches or Setting by Toledo-Software) |
2/24/2014 6:31 PM | |
Posts: 8946 Rating: (999) |
Doublecheck if cable, plugsand termination is OK. Is GSD file correct? |