11/9/2019 2:44 AM | |
Posts: 6 Rating: (0) |
I'm trying to communicate to a device through RS232 using Siemens S7317 with CMPTP module and step7 V5.6. Got the Send_p2p block ver 1.3. The problem is I get the status of SendP2P as error and error code is 8281 which is negative acknowledgement while writing, but not sure what's the issue in the input port. Attaching the pic of instance db, code snipped and the hw config. Attachmentcmp2p.zip (35 Downloads) |
11/13/2019 10:02 PM | |
Posts: 6 Rating: (0) |
Attaching here the parameters, if that's what you meant ? |
11/14/2019 2:23 PM | |
Posts: 6 Rating: (0) |
Attaching the extended pars, general. Attachmentptp_pars.zip (28 Downloads) |
1/17/2020 5:03 AM | |
Posts: 6 Rating: (0) |
Any ideas are welcome ! |
Follow us on