5/10/2021 9:59 AM | |
Joined: 2/19/2013 Last visit: 7/25/2024 Posts: 16 Rating: (1) |
Dear all , I have the same problem with V16. I have a new comfort panel 6AV2124-UOC02-0AX0. The device is delivered with version image 16.0.0.3. When I try to download, it gives me the message that I I should install the correct panel images / panel images incompatible. In TIA you can ony select V16.0.0.0 as an image for the device. 4 weeks ago I had the same problem with a 2nd display, I changed the panel version in 15.1 ( in V16 that is ) and downgraded the display to make it work... If anyone has a solution to this I would be very glad to hear it :-) Greetings ! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2021 14:21:59New subject after splitting |
|
5/20/2021 9:17 AM | |
Posts: 1 Rating: (0) |
I am having the exact same issue. Is this some kind of bug in TIA? |
5/20/2021 11:16 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hello, Please have in mind, that you have a Comfort panel. You have to use the image of a Comfort panel, see: Image Downloads for HMI Operator Panels Download and install the images for Comfort panel (Not unified Comfort panel ) Best regards, Wizard |
9/9/2021 1:33 PM | |
Joined: 3/1/2018 Last visit: 3/7/2024 Posts: 9 Rating: (1) |
I have the same problem with TP1500. I have tried downloading latest images but still same problem. Anyone knows anything? |
Follow us on