3/10/2014 2:57 PM | |
Posts: 14 Rating: (0) |
I find the manual and examples for the "command interface" on the Step7 installation DVD. \_Manuals\English\Command Interface On this DVD is one project. I have converted this project from Visual Basic 6.0 to Visual Studio 2008. How can I use this project for example: create new Step7 project or do something easy. I need some working example. Could you tell me, how do it? AttachmentExamples.NET3.zip (474 Downloads) |
Last edited by: GrasserF at: 3/11/2014 8:44 AMnew subject after splitting from /tf/WW/en/Posts/72100 |
|
3/20/2014 2:59 PM | |
Posts: 14 Rating: (0) |
Dear Mrsmoky I have added this: Call Modu.Modules(2).AddSubSystem("my_pn", 1) Now is better. I have PROFINET network and my CPU is connected to this network. But I don't have PROFINET IO system (see right side attachment, where I add this PROFINET IO system in Step7 manually). Without PROFINET IO system I can't addET200S (6ES7 151-3AA23-0AB0). Could you tell me, what I should change?
|
3/21/2014 9:02 AM | |
Posts: 14 Rating: (0) |
Dear Mrsmoky I would like do this from command interface. It is possible?
|
Follow us on