Industry Online Support
Technical Forum
10/27/2009 2:47 PM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hi Delphoe , commissioning wizard runs automatically after PCS7 installation and rebbot PC. if not, you can always change manually from SIMATIC NET -> Configuration Console. very strange you don't have it beccause PCS7 automaticallyinstall it. Regards |
10/27/2009 10:21 PM | |
Posts: 2661 Rating: (279)
|
Hi Delphoe, This is normal behavior. That is, from PCS7 V6.1 onwardsthe Simatic Net PC Configuration Wizard tool doesn't get installed. This wizard was a "feature" in PCS7 V6.0 only. Probably this can be installed using a separate Simatic Net CD but you should notattempt this on top of PCS7. Moreover it is not required. For PCS7 V6.1 and highergood guidelines are availablein the following manual: SIMATIC Process Control System PCS 7 Compendium Part A - Configuration Guidelines Following FAQ is valid only for PCS7 V6.0: Which settings have to be made on an Engineering Station (ES) and in the SIMATIC PCS 7 V6.0 project so that the project can be loaded and commissioned with all computers (ES, OS Server, OS Terminal)? Regards |
10/29/2009 9:03 AM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hi Delphoe , you already have "WinCC Aplication..." on index nr.1; only one WinCC has to be configured in accordin with your station. Once configured, it will be no more available (because you can't use twce in same station). read manual in PCS7 documentation"PCS 7 - Configuration Manual Engineering System" & "PCS 7 - Configuration Manual Operator Station" for basic info like that. Or ask for a training to your local Siemens Service About CP1613 card: use Simatic Net inside PCS7 DVD (abslutely don't use Simatic Net CD coming with the cards) Regards |
Follow us on