4/4/2016 11:18 AM | |
Joined: 10/4/2015 Last visit: 3/16/2024 Posts: 4 Rating: (0) |
Dear Siemens, I have a question. Can i do communicate with s7-200 in both ppi and ethernet with CP243-1IT? i do two networks : one s7-200 master- 6 slaves s7-200 ( PPI netr/netw). and one networks : s7-200 master cp243-1IT - s7-200 master Cp243-1IT. thanks and best regards Le Huy
------------------------------------------------------------------------------------------ following this enclose emage, can exchange data between s7-200 cpus when communicate both two protocols in one cpu? |
Last edited by: Min_Moderator at: 4/4/2016 12:33:07 PMNew subject after splitting Last edited by: Min_Moderator at: 4/4/2016 3:57:04 PMAdd attachment Last edited by: ADAUTOMATION1234 at: 4/5/2016 4:22:15 AM |
|
4/13/2016 6:25 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello AD Automation; You will find almost everything you need as far as basic information on the s7-200 in the following manual:
S7-200 System Manual
https://support.industry.siemens.com/cs/ww/en/view/1109582
Additionally, these FAQs may provide more detailed networking information:
How is data exchanged between two SIMATIC S7-200 devices in PPI mode?
https://support.industry.siemens.com/cs/ww/en/view/370000
Micro Automation: Networking automation systems via Industrial Ethernet (MAS 14)
https://support.industry.siemens.com/cs/ww/en/view/21062588 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on