8/13/2013 4:18 PM | |
Posts: 3609 Rating: (29) |
Import of a technical question of the User AutoGen_424753
|
8/13/2013 5:12 PM | |
Joined: 1/28/2012 Last visit: 9/15/2023 Posts: 519 Rating: (83) |
[quote user="Import-User-1"]Import of a technical question of the User AutoGen_424753 [quote user="AutoGen_424753"]I am facing an issue while using CPU 1214C while communicating directly with WinCC. Can pl. guide me which other scada software i can use to communicate with this processor. Which version do you have for Wincc. ? From Wincc 7.2 onwards. , The communication driver for S7-1200/1500 is available. . But if you have older version of Wincc such as Wincc 7.0 then you may find questions related to this. . Please copy paste below link for similar discussion. . In that questions, The idea given was use of OPC server using Simatic PC Access through which DB1 of S7-1200 can be accessed through OPC in Wincc. . /tf/WW/en/Posts/46335 Hope it helps. . |
Last edited by: Pranav J. Bhagat at: 8/13/2013 5:28 PMLast edited by: Pranav J. Bhagat at: 8/13/2013 5:14 PMRegards, |
|
8/13/2013 5:35 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, Please have a look at How do you connect a PC station to an S7-1200 with OPC? Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
2/19/2018 12:41 PM | |
Joined: 6/19/2017 Last visit: 4/19/2024 Posts: 7950 Rating: (162) |
New question published by kazi_engineer is split to a separate thread with the subject Communication problem with 1214c with wincc. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on