6/19/2019 11:33 PM | |
Posts: 3093 Rating: (322)
|
Hello, Regards, |
6/21/2019 9:56 AM | |
Posts: 3093 Rating: (322)
|
Hello, Regards, |
6/21/2019 9:39 PM | |
Posts: 3 Rating: (0) |
Sir, What are all the hardware required to establish communication between the two (S7 - 300 & EM 6436) |
6/21/2019 11:11 PM | |
Joined: 9/27/2006 Last visit: 3/28/2024 Posts: 12249 Rating: (2660) |
Hello srini; The usual (recommended by Siemens) way to connect a S7-300 to a Modbus RTU slave is to use a CP 341 along with a Modbus RTU master loadable driver and external dongle. This combination can be quite expensive. You will find complete information in this manual: https://support.industry.siemens.com/cs/us/en/view/1220184 An alternative has been developed by our friend TIBI68. It allows the use of a less expensive serial comm processor, the CP 340, and the functions are freely available from this thread: As you can see in this very long thread, TIBI68 himself has helped improve his function blocks as Siemens programmers have used them, and he still offers support when needed. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/22/2019 00:12:53 |
|
Follow us on