11/2/2008 6:52 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, I would stay with S7 connections. You try to configure a connection, and theerror that you get is because a configuredS7 connection cannot be unspecified. It would be enough to add a copy of the HWConfig of your new CPUs in the old project. Of course you must configure exactly the same in your new project. To avoid errors doing that, You could also define a multiproject. You add your old one and the new one in the multiproject. And you create S7 connections between the modules located in the projects of the multiproject. See: http://support.automation.siemens.com/WW/view/en/14844050 and: http://support.automation.siemens.com/WW/view/en/18652631 |
Last edited by: edr at: 11/2/2008 6:53 PMBest regards |
|
11/3/2008 12:04 PM | |
Posts: 2 Rating: (0) |
Thanks for your help. More information would be much appreciated if you can find it. Regards Mike |
11/4/2008 11:38 AM | |
Posts: 5822 Rating: (412)
|
Dear Mike, I am sorry, I just talked to Customer Support and they said that they removed the sample they had because they experienced too many problems with customers so they prefer to have no sample about it. J_Bell |
Last edited by: J_Bell at: 11/4/2008 11:38 AM |
|
Follow us on