5/11/2017 8:42 AM | |
Posts: 25 Rating: (0) |
Hello, Thanks for reply. Here are 2 Manuals about SPBL program code of the SATO CL4NX. https://www.satoamerica.com/uploads/files/datasheets/E%20Pro%20Programming%20Reference.pdf http://www.htz.com.tw/products/cl4nx/manual/CL4NX_Programming%20Reference_ENG_01.pdf |
This contribution was helpful to1 thankful Users |
5/11/2017 11:05 AM | |
Posts: 25 Rating: (0) |
Hello, Thanks for reply me a lot and fast. I have try to take a array of char instead of a string like you said but i stil don't understand how i need to make ma code. Like you can see in the datasheet i used the code like they said but need i to convert this code into an other way or do i need it to do like in picture 1. And also do i need a STX and a ETX my english is not very well so i don't understand the datasheets very good what i need to do with the code. I have also put mij program in pdf in the attachment so you can see what i try to do. I hope you can help me. I need to fix this. :( I also don't understand what you mean with take <ESC> as 1 byte. How can i do that ? AttachmentPLC.zip (148 Downloads) |
Last edited by: ArneVDS4796 at: 5/11/2017 11:07:54 AM |
|
5/11/2017 2:23 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Hello, you're welcome. Good luck to next projects. |
With best regards... |
|
2/6/2018 10:52 AM | |
Joined: 12/4/2014 Last visit: 2/17/2022 Posts: 3 Rating: (0) |
@ArneVDS4796, can you upload a sample program? I would like to see final "send DB". Thanks. |
Last edited by: konec_ja at: 2/6/2018 10:52:57 AM |
|
Follow us on