5/27/2014 9:48 AM | |
Posts: 17 Rating: (0) |
Hello, you are right I did the inversion between Min and Max, but even corrected the problem is not solved. The Thermocouple is type J |
7/24/2014 3:30 PM | |
Posts: 17 Rating: (0) |
Hello, I'm pleased to inform and confirm that with the appropriate base-unit, everything is working better!! |
This contribution was helpful to1 thankful Users |
9/28/2015 2:05 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi AMS Automation, have a Look into the Manual Collection to get the information which BaseUnit is the right for your module. See the Basic Information->decentral peripherie system chapter 3.1 hope this helps, regards, |
FCK WAR! |
|
Follow us on