2/27/2019 6:50 PM | |
Joined: 11/2/2017 Last visit: 4/10/2024 Posts: 18 Rating: (0) |
Hello esoy doing a communication between Logo and IOT2020, well for the moment as you can see in the picture that I attached, I can read all the DB memory! of the logo and write also, but I get the following problem: I can only change the entries in logo with inject, since it is a true - false, with pin 2 of gpio that I have in the flow, when I connect it to node s7 output does not do anything in the logo. another thing that happens is that on the logo side, the signal does not stay connected although on the iot this. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/28/2019 6:26:27 AMNew subject after splitting |
|
2/27/2019 6:52 PM | |
Joined: 11/2/2017 Last visit: 4/10/2024 Posts: 18 Rating: (0) |
My flow
AttachmentFl.txt (140 Downloads) |
2/28/2019 8:20 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, the reason that the GPIO Pin does not write anything to the LOGO! is that it provides the data in format "number" (which is an integer). You have to change it to boolean. What do you mean with "the signal does not stay connected"? Best regards! Attachmentconversion.txt (120 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
3/1/2019 12:55 PM | |
Joined: 11/2/2017 Last visit: 4/10/2024 Posts: 18 Rating: (0) |
Hello, I pass a link with 2 video captures, one of the red node's side, where you can see how the GPIO2 changes and the output of S / y in the other. You can see the part of the Logo where the network input NI1, It turns on and off by itself, it does not work like a switch, it just makes a pulse. Someone knows what may be due, since I do not find logic. link drive: Attachmentfiles.zip (123 Downloads) |
Last edited by: Jen_Moderator at: 3/1/2019 2:00:11 PMRemoved link and added file as an attachment. |
|
Follow us on