3/21/2010 5:16 PM | |
Posts: 691 Rating: (36) |
Better check the communication defined for the WinCC Flexible Runtime and match the same in the Set PG/PC Interface Setting |
3/22/2010 5:03 AM | |
Posts: 13 Rating: (0) |
yes.. i've checked access path S7 online, i set same in PG/PC interface.. is it possible to communicate with PC/PPI cable..? |
3/22/2010 5:36 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Naveen, Look at What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options? Hope this helps. Best regards, Hristo Mihalev |
3/22/2010 2:05 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already discussed in the following thread Connection between winCC flexible runtime and S7 200. Best regards O_Moderator |
Follow us on