7/15/2020 5:31 PM | |
Joined: 9/28/2018 Last visit: 3/6/2024 Posts: 14 Rating: (0) |
Hi, I want to set up a communication between two PLCs - S7-300 CPU 317C-2 PN/DP and ET200S CPU IM151-8F PN/DP. I just need to read one real number from PLC 1 and send it to PLC 2 use TIA V15. I create I-device with ET200S CPU IM151-8F PN/DP but Faulty configuration. Plase help me (see attachment). Thank you.
AttachmentCommunication between S7-300 and ET200S.zip (92 Downloads) |
7/16/2020 6:13 PM | |
Joined: 9/28/2018 Last visit: 3/6/2024 Posts: 14 Rating: (0) |
Hi Christoph, If I use PLCSIM, it will get the same error. If I use real PLC then error message as attached file.If I do not use I-device, there will be no error.Plase help me. Thank! Regards AttachmentError.zip (68 Downloads) |
7/16/2020 6:52 PM | |
Joined: 9/28/2018 Last visit: 3/6/2024 Posts: 14 Rating: (0) |
Hi Duris_I, I have set the password, but the error is still there. Best regards |
Follow us on