11/20/2009 4:14 AM | |
Posts: 4 Rating: (0) |
hi Ammy |
11/20/2009 4:42 AM | |
Posts: 4 Rating: (0) |
hii rogermann |
5/22/2014 9:56 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello M_syrian, Are looking for this..... How can you link WinCC to S7 PLCSIM? this will help u to setup the WinCC with PLC Sim |
Last edited by: Ammy at: 5/22/2014 9:57 AMAmmy |
|
5/22/2014 10:52 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
HiM_syrian In PC/PG interface just use PLCSim (TCP/IP) since all your tags has been installed in TCP/IP connection. Also, check the connection in PLCSim connection drop down window to be PLCSIM(TCP/IP)
Did you followAmmy sugestion belowand did not work well kindly.
Finaly, check all IP addresses for PLC and PC station, it must be the same network. Hope this helps, waiting for your reply. |
Best Regards |
|
5/22/2014 2:14 PM | |
Posts: 9 Rating: (0) |
kindly you see the attchment of my project setting when i select ISO not possiable to dwonlaod and wincc no see the PLCsim your kind advice regards Attachmente.zip (338 Downloads) |
12/19/2016 11:53 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Xurshid is split to a separate thread with the subject No connection between PLCSIM V5.4 and WinCC 7.0. Best regards |
Follow us on