6/16/2009 12:53 PM | |
Posts: 163 Rating: (0) |
Can anybody help me with a sample program of FC50 and FC60 using s7 fault tolerant connection.Need to exchange data from both the stations. |
6/23/2009 1:05 PM | |
Posts: 163 Rating: (0) |
is there any restrictions on calling the number of times the FC5 and FC6 are to be used? |
6/23/2009 2:51 PM | |
Posts: 5822 Rating: (411)
|
Hello, I am sorry, I am lost a bit... may I try to resume first. |
Last edited by: J_Bell at: 8/27/2009 11:53 AM |
|
6/24/2009 6:52 AM | |
Posts: 163 Rating: (0) |
How do I chk the communication between these two stations after using get/put function using S7-PLCSIM |
Follow us on