1/7/2013 3:14 PM | |
Posts: 5 Rating: (2) |
I SEARCHED THE DOCUMENTS ABOUT COMMUNICATE TO WINCC AND ALLEND BRADLEY COMPACT LOGIX LX32 PLC.FINALLY I DID AND I WANT TO SHARE THIS. YOU CAN FIND PICTURE OF THE COMMUNICATION CHANNEL,CHANNEL PARAMETERS AND TAG NAMES AND ADRESSES. I TRY TO EXPLAIN HOW I DID. 1- AT FIRST WE MUST TO ADD ALLEN BRADLEY ETHERNET IP CHANNEL DRIVER. 2-AFTER ADDING AB ETHERNET-IP CHANNEL WE CREATE TO PLC CONNECTION.I CREATED THIS CONNECTION IN THE "Allen Bradley E/IP ControlLogix` channel/ 3-SETTING PLC IP PARAMETERS.WE ENTERING PLC TCP/IP ADRESSES INTO THE IP ADRESS PATH.Communication Path must be 1,0 4-CREATING TAGS. TAG ADRESSES MUST BE SAME LIKE ALLEN BRADLEY PROGRAMS.DONT FORGET TO ADD THE PROGRAM NAME TO THE TAG NAME.THE PART OF THE BEFORE : IS PROGRAM NAME. AttachmentCommWinccAllenBradley.zip (1517 Downloads) |
This contribution was helpful to5 thankful Users |
6/13/2013 9:03 PM | |
Posts: 3 Rating: (0) |
Thanks, it help me a lot |
This contribution was helpful to1 thankful Users |
4/3/2015 2:09 PM | |
Joined: 11/8/2011 Last visit: 11/28/2023 Posts: 8 Rating: (0) |
Dear Can u try to understand me the binary type tag parameter |
Follow us on