7/1/2010 5:57 AM | |
Joined: 5/6/2010 Last visit: 3/13/2023 Posts: 11 Rating: (0) |
I have to communicate to sinamics G130 DRIVES (3 NOS) OVER PROFIBUS WITH S7400 H CPU 414H i am using ycoupler. |
7/6/2010 5:50 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
What I am understanding is you need GSD file for G130... Check following SINAMICS Support Package (SSP) SINAMICS V2.6.2 for SINAMICS drives G130/G150/GL150/GM150/S120 and S150 suitable for the S7 Technology V4.1 SP1 This is what you need to communicate drive and PLC.... Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/6/2010 5:56 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
HI mbm, are you looking for the following, MICROMASTER 4 & SINAMICS G Function block (FC14) to control an MM4 via Profibus-DP Directly controlling a MICROMASTER 4 / SINAMICS G120 / SINAMICS G120D from a SIMATIC HMI station via PROFIBUS-DP and PROFINET Enjoy, |
Ammy |
|
This contribution was helpful to1 thankful Users |