4/12/2012 11:20 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Raheel, For establishing connection between S7 200 PLC and PC via USB interface, you have two possibilities. 1. 6ES7901-3DB30-0XA0 2. 6ES7972-0CB20-0XA0This cable is more expensive than the previous one because you can use it to communicate to S7 200 and S7 300 / S7 400 as well. Also Have a look on the How can I select USB-PLC Data Cable ?Please Checked your S7-200 PLC No. if Should Be CPU 224, or you will find on the Module MLFB no. to find the Correct way on the Siemens Website.Here is the link for the S7-200 Manual |
Ammy |
|
4/12/2012 11:24 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, You need PPI to communicate with a 200 series. For if it's still available you need to contact your local Siemens Rep. https://www.automation.siemens.com/partner/index.asp?HTTPS=REDIR®id=WW&lang=en&comptcid=o There is no information about CN types here in europe. For the manual i can only refer to the S7 200 system manual. http://support.automation.siemens.com/WW/view/en/1109582 The CN CPU will be pretty mutch the same. Regards, Marcjan |
Last edited by: Marcjan at: 4/12/2012 11:25 AMProblem solved? |
|