11/8/2012 5:59 AM | |
Posts: 40 Rating: (0) |
i below error.. when i flash the driver it came okay and led function |
11/8/2012 6:01 AM | |
Posts: 40 Rating: (0) |
when i test hardware OK.led flashing .i check on hardware..seem working (divice manager on system) |
11/8/2012 6:02 AM | |
Posts: 40 Rating: (0) |
attach was project i was working on..and msg when try to connect with WICC |
11/8/2012 7:18 AM | |
Posts: 40 Rating: (0) |
sorry it suppose to be CPU 313c-2dp (s7-300) my mistake on that .. im using step7 5.5 and using wincc 2008 sp3. |
11/8/2012 11:15 AM | |
Posts: 40 Rating: (0) |
still get the same error..as screen shot 3.. |
11/8/2012 11:18 AM | |
Posts: 1064 Rating: (72) |
This might be a silly question but are you end of line switches set properly? |
11/8/2012 11:39 AM | |
Posts: 1064 Rating: (72) |
did you try to auto detect the bus parameters under set pg interface , properties then start network detection ?? |
11/8/2012 11:48 AM | |
Posts: 40 Rating: (0) |
Yes i did..but result same cant find Partner .. |
11/8/2012 11:54 AM | |
Posts: 1064 Rating: (72) |
have you tried to connect to another plc with your pc or a different cable |
11/8/2012 11:59 AM | |
Posts: 40 Rating: (0) |
..No ..but i do know this new PLC s7-300 and modifaction project on wincc where by we add new machine to it ..currently plant running in manual mode as well.. |
11/9/2012 3:37 AM | |
Posts: 40 Rating: (0) |
this was the error i m getting cant see any bus node |
11/9/2012 7:02 AM | |
Joined: 1/8/2008 Last visit: 4/11/2024 Posts: 264 Rating: (45) |
Hi, i hope you have Windows 32Bit !? in Windows 64Bit you can't use CP5611 (look at support ID 61630624) |
11/9/2012 8:26 AM | |
Posts: 40 Rating: (0) |
HI sir i just confirm it was windows 32bit..using window Xp pro.. |
11/15/2012 7:43 AM | |
Posts: 40 Rating: (0) |
here is the attach screen shot ..of 6 pic what i did n the result |
11/15/2012 7:44 AM | |
Posts: 40 Rating: (0) |
pic2 |
11/15/2012 7:45 AM | |
Posts: 40 Rating: (0) |
|
11/15/2012 7:45 AM | |
Posts: 40 Rating: (0) |
|
11/15/2012 7:46 AM | |
Posts: 40 Rating: (0) |
|
11/15/2012 11:50 AM | |
Joined: 1/8/2008 Last visit: 4/11/2024 Posts: 264 Rating: (45) |
Hi, test the CP5611 in another PC or reinstall regards |
11/15/2012 1:14 PM | |
Joined: 1/8/2008 Last visit: 4/11/2024 Posts: 264 Rating: (45) |
delete CP in hardware-manager und restart windows |
Follow us on