4/1/2018 3:38 PM | |
Joined: 2/8/2009 Last visit: 11/3/2023 Posts: 9 Rating: (0) |
Good morning everyone. I'm having trouble finding the communication driver for Siprotec Relay:7SJ80 - FW: 4.74.05 Could you tell me where I can find this driver, or if there is a way to update the firmware of the relay. I can not record the parameters in the Relay because of the incompatibility between the Driver version and the Firmware version. Digsi version that I use is4.90 Thank you all for your help. ------------------------------------------------------------------------------------------ |
Last edited by: Chicão at: 4/1/2018 3:46:02 PMLast edited by: Jen_Moderator at: 4/3/2018 6:34:07 AMNew subject after splitting |
|
4/2/2018 7:11 PM | |
Joined: 5/13/2012 Last visit: 1/17/2024 Posts: 179 Rating: (1) |
hallo sir you can download all previous firmware from the below link .and it is compatible with the digsi 4.90 . https://support.industry.siemens.com/cs/us/en/view/109749184 you have to register to access the download file. |
Last edited by: Jen_Moderator at: 4/3/2018 6:35:51 AMOptimized link. best regards |
|
4/3/2018 3:57 PM | |
Joined: 10/9/2007 Last visit: 4/22/2024 Posts: 1239 Rating: (115)
|
for older Firmware you have to contact Support.energy@siemens.com |
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on