6/2/2011 5:51 AM | |
Posts: 272 Rating: (4) |
Dear All, I want to know that can we Run an OS Client simultaneously with a Thin client. I have installed Web Acess in OS Client. |
6/2/2011 6:45 AM | |
Posts: 212 Rating: (12) |
Dear Prats, What is system configuration? Which versions of WinCC / PCS7? |
6/2/2011 7:16 AM | |
Posts: 272 Rating: (4) |
Hi ABN , I am using WinCC V7.0 |
6/2/2011 7:20 AM | |
Posts: 212 Rating: (12) |
Configuration? |
6/2/2011 7:34 AM | |
Posts: 272 Rating: (4) |
We have Red Server Client Architecture, now we want thin client to be connected to a client. The client will act as a web navigator server. |
6/2/2011 7:55 AM | |
Posts: 272 Rating: (4) |
Dear ABN, We are not using PCS 7 in the current project. |
6/2/2011 8:07 AM | |
Posts: 212 Rating: (12) |
Doesnt matter. You consider the previosu thread as WinCC Client. You must refer the same file available with installation or plz find attachment AttachmentPC Configuration for WinCC 7.0 SP1.pdf (147 Downloads) |
6/2/2011 8:14 AM | |
Posts: 103 Rating: (6) |
Dear Prat, |
This contribution was helpful to1 thankful Users |
Follow us on