11/3/2014 9:27 AM | |
Posts: 6 Rating: (0) |
Hi I have got a LOGO of type 1P 6ED1052-1CC01-0BA8. My installed version of Logo!Soft Comfort is V8.0.0(2014-06-29 16-25). It is running in virtual achine (VMware player). I have a trouble with connection to LOGO 8 from my PC - I cannot transfer program to/from this LOGO etc. Each time when I want to connect to LOGO 8, I get this message (screen_1.png). Ping from PC to LOGO 8 works, ping from LOGO 8 to PC works. Even when I create netwrok projekt in Logo!Soft, SW can detect LOGO 8 online (screen_2.png) However when I try to connect to it I have problem. I have also tested logo 7 (6ED1 052-1MD00-0AB07) with the same PC and with same Logo!Soft Comfort V8.0.0 - in this case to communication works without any problem. It is strange. Can you help me ? Thanks in advanced Attachmentscreens.zip (848 Downloads) |
11/3/2014 2:51 PM | |
Posts: 6 Rating: (0) |
Hello, yes Logo works in an admin mode, despite I'm not able to connect to it |
12/5/2014 11:07 AM | |
Joined: 12/4/2014 Last visit: 12/22/2023 Posts: 2 Rating: (0) |
Hello Also have the same problem Logo Soft Comfort v8 installed on physical pc Win Xp Pro SP3 Logo1 and 2, are in the admin-mode Have try restart LSC V8 and PC after the warning message but the problem persist Communication with LSC V7 is working without any problem I have upload a video in .zip file with configuration settings ip, subnet mask and lan interface I can not think anything else Please help Attachmentcommunication problem logov8new.zip (701 Downloads) |
Follow us on