Industry Online Support
Technical Forum
7/24/2014 4:41 PM | |
Posts: 1 Rating: (0) |
Dear Experts, I'm involve in a project who decides to use DCS Yokogawa with Profibus master ALP111. We know that master only accept DPV0 messages. Some time ago we did a question about this thread: /tf/WW/en/Posts/79538 The solution for our problem was: 1)Disable watch dog /plc dcs monitoring in simocode. 2)Disable time stamping in simocode 3)Disable diagnosis triggered by fault & event in Simocode. We changed the configuration and it works. But this days we have a similar problem, but when we energize Simocode this send a message of 15 bytes (it's configured only to send 10 bytes), the DCSrecognizesas parity error andloses communication in the segment. This happen only with one of Simocode on the net.We are using GSD v1.5. The message was captured using Profitrace: 68 0D 0D 68 01 08 08 42 00 00 00 00 00 00 00 FF We think that message could be Device Diagnosis but we aren't sure (Manual page B-10). When the Simocode send a message like this? Anyone have had a similar situation? Someone could give us any advice? Attachment is Simocode configuration. Thanks in advance. Best regards Felipe
Attachment5150-PP-008-M01rev3.zip (206 Downloads) |
Follow us on