6/12/2014 1:49 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello tekisyen_sistem; There are no Modbus TCP blocks available from Siemens for the S7-200. One possible solution: You could purchase the Modbus RTU library for MicroWin and then use a gateway from Modbus TCP to Modbus RTU to connect with your Schneider PLC. See here for Modbus RTU instructions: How do you implement MODBUS communication with S7-200? Hope this helps, Daniel Chartier |
2/25/2016 1:30 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by mrbum is split to a separate thread with the subject S7 200, error: 'unknown address'. Best regards |
Follow us on