7/20/2010 1:54 PM | |
Joined: 10/7/2005 Last visit: 5/14/2024 Posts: 3005 Rating: (1048)
|
Hello dstudio the short answers is that you can do safety related communication between two F-CPU's via a PN/PN coupler. There are a few things to "look out" for though and the best place to start is the S7 Distributed Safety - configuring and programming manual(see especially chapter 8.2 and 8.6) and I suggest to have a look too at theSafety: Calculation of the monitoring and response times by using the Excel table s7fcotib(itgreatly helps in calulating the correct Timeout values for the F related comms). I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
7/24/2010 8:53 AM | |
Joined: 8/24/2006 Last visit: 4/12/2024 Posts: 148 Rating: (9) |
Ok Thank you!!! |
Follow us on