5/3/2017 1:00 PM | |
Joined: 6/30/2014 Last visit: 4/17/2024 Posts: 456 Rating: (86)
|
Hello Adrian, from your last screenshot I can see that your CLS, your ComosLicenseServer is working well, that your Dongle has been found, that your client config file has been edited. I see in your config that the CLS-Name has been entered there: are you able to ping that PC-Name, does it answers? If not, can you ping it's IP-Address instead? If so, please enter the IP-Address into the config file (instead of the CLS-Name) and try again. Does the Client reach the CLS over the network? Which ID did your Ticket at the Support, which number does it has? It usually does not takes days to get an answer or even a solution from there. Please try this: start (without installation, only start) the debugview from Microsoft on your client; than rebuild the issue, save the log file and send it to the Support mentioning the IR number, the ticket number. Also, please send a copy of the "Data" directory of the affected CLS to the Support: you find it in the installation path of the CLS; please zip it and send it to them. By the way: a Server license, is not the same of a local one; just in case you got the wrong type for your purpose, please get in touch with the sales person/license admin which have provided you with a license file. Also, the license file is always a XML file, never a TXT file for COMOS, please make sure to use the license file, not the text file which you have received. I'm sure you will manage to solve this very fast, I'l like to help also. Just in case other users have such an issue: please open a ticket at the Support, here you see the FAQ which shows how to open a ticket at the COMOS-Support.. All the very best, SuperPippo |
5/8/2017 2:18 PM | |
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating: (42) |
Hi Adrian, Please post the answer, if you solved it. -- Regards Dinesh K |
5/31/2017 6:43 AM | |
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating: (42) |
Hello adriantaw, Great to hear. -- Regards Dinesh K |
1/3/2020 2:56 AM | |
Posts: 4 Rating: (0) |
Hi, Can you suggest me the steps for license type "Local"? I got the same error ErrorCodes_LS: -2000 -1. |
Last edited by: Nanasaki at: 01/03/2020 02:57:30 |
|
Follow us on