5/30/2018 2:50 PM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Dear medommido, For the hardware part, please read carefully the link below: Important Notice for the usage of the failsafe SIMATIC S7-1200 CPU’s in combination with the SIMATIC S7-1200 Standard Signal Modules For the project part, depending on the old CPU firmware version and the TIA Portal version under which your old project was created, the steps for device change and project migration may vary. For example, if in the project your old CPU is of FW 1.0, you need to change it first to FW2.0/FW3.0 and then you can select an F-CPU of FW4.x. For project migration, please refer to the link below: Migration Tool TIA Portal Best regards, Yu-wen |
This contribution was helpful to1 thankful Users |
6/2/2018 11:36 AM | |
Posts: 4 Rating: (0) |
Dear Yu-wen Tang, Thanks too much for your help. your Answer was very helpful. |