Industry Online Support
Technical Forum
9/1/2009 2:36 PM | |
Posts: 81 Rating: (0) |
Hello, Trying to compile a Plc that belongs to a multiproject I got those compilations errors. See files attached. I have checked the following link and I got the same error The only thing I have done is to add a new block in a CFC and delete it. I have loaded a previous backup and I have the same problem with the same PLC, the other two that belong to the multiproject work properly. I also have loaded an old backup of the C drive to confirm is not a software problem. Any idea Thanks AttachmentCompile Errors.zip (130 Downloads) |
9/1/2009 2:53 PM | |
Posts: 81 Rating: (0) |
More information If I check the consistendy of that project, I get the attached error
|
Follow us on