3/2/2020 3:04 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
Hello, and which Et200S exactly? |
3/2/2020 3:08 PM | |
Posts: 3 Rating: (0) |
ET200S IM151-8 PN/DP,192kByte,SIEMENS 6ES7151-8AB01-0AB0 Thanks |
3/2/2020 3:27 PM | |
Joined: 9/27/2006 Last visit: 5/5/2024 Posts: 12257 Rating: (2666) |
Hello leo; The IM 151-8 is a ET 200S CPU with a Profinet interface. To act as a Profibus-DP master it requires an additional module, as shown in the screenshot below. What software version are you using to program this CPU? And how familiar are ou with the ET 200S hardware, and wih Profibus-DP configurations in general? Your ET 200S CPU is enabled for Modbus TCP communications over its Profinet interface; communictaion function blocks are available in the program: How do you establish a Modbus/TCP communication from a SIMATIC S7-300/S7-400 and where can you find further information? (Note: The IM 151-8 is considered a S7-300 CPU). https://support.industry.siemens.com/cs/ww/en/view/22660304 I belowhave added to the screenshot an example of connexion between an IM 151-8 and a Modicon PLC, taken from this document: Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 03/02/2020 15:38:13 |
|
Follow us on